• No : 21079
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

The speed response of the vector control (Both with PG/without PG) is improved by more than two times compared to the A700. Is the current response also improved at the same rate?
Category : 

Answer

Yes, the current response is also improved at the same rate.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800