• No : 21106
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Can other manufacturers' magnet motors be used?
Category : 

Answer

By performing offline auto tuning, other manufacturers' IPM, SPM motors can be used under PM sensorless vector control. * When an other manufacturers' magnet motor is used after auto tuning, the starting torque is limited at 50% and zero speed operation or simple positioning control cannot be used. (Tuning may not be available depending on its motor characteristics.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800