• No : 21140
  • Release Date : 2018/08/22 16:26
  • Print

FR-BMF

The Instruction Manual instructs includes the following description: "Set Pr.72 "PWM frequency selection" to 2 kHz or less". What happens when 3 kHz or more is set?
Category : 

Answer

The inverter may be broken due to the temperature rise of the internal parts.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option