• No : 21181
  • Release Date : 2018/08/22 16:26
  • Print

FR-B3

The carrier frequency can be set in Pr.72 (PWM frequency selection) for the FR-B, but it cannot be set for the FR-B3. What is the carrier frequency (kHz) set for the FR-B3?
Category : 

Answer

The carrier frequency for the FR-B3 is 2 kHz. For the low noise type FR-B3-N, it is 14.5 kHz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option