- No : 21185
- Release Date : 2018/08/22 16:26
-
Print
Brake sequence function
The instruction manual includes the following description: "Set the acceleration/deceleration time to 1 s or more". What is the corresponding value (Hz) to 1 s?
- Category :
-
Answer
The value of Pr.20 (Acceleration/deceleration standard frequency) is corresponding to 1 s. (Initial value: 60 Hz)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700