- No : 21380
- Release Date : 2018/08/22 16:27
-
Print
Remote operation of the inverter
I want to perform remote operation of the inverter with the different enclosure contact. How long can I extend the control circuit and input signal (contact) circuit? (Example: 100 m etc.)Also, what is the voltage of this circuit?
- Category :
-
Answer
The wiring length of the start signal (STF etc.) is 30 m or less.
The circuit voltage of the control input signals (terminal STF etc.) is 24 VDC and the voltage when contacts are open is from 21 to 27 VDC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500