• No : 21389
  • Release Date : 2018/08/22 16:27
  • Print

Selection method of the reactor

Why and how should I select the reactor between the inverter and motor?
Category : 

Answer

For the use of the 400 V class inverter, the surge voltage suppression filter FR-ASF is provided to suppress the surge voltage occurred at the motor terminal voltage.
Select reactor according to the motor capacity.
Product Name
Inverter, magnet motor drive
Series
Option