- No : 21414
- Release Date : 2018/08/22 16:27
-
Print
EMC countermeasure
Let me know precautions when exporting equipment using the inverter to the United Kingdom, U.S.A., or Canada.
- Category :
-
Answer
To conform to the EMC Directive when exporting to an EU country, install the filter that conforms to the EMC Directive on the inverter, and take measures according to Mitsubishi "EMC guidelines".
Note that the entire equipment with the inverter built in must conform the to the EMC Directive.
When exporting to U.S.A. or Canada, power drive devices for industrial application such as inverters are not subject to the EMC regulation (FCC and others) and there is no special precaution regarding EMC.
Our inverter products have acquired the UL and cUL certification.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500