- No : 21416
- Release Date : 2018/08/22 16:27
-
Print
Frequency setting
How can I set the inverter frequency to 120 Hz using the potentiometer of the FR-E520?
- Category :
-
Answer
Ensure that the inverter is in the PU operation mode and stopped, change the following parameters:
1. Read Pr.923 (Built-in frequency setting potentiometer gain).
2. Change it to 120 Hz, and press and hold the SET key for 1.5 seconds.
3. Turn the built-in potentiometer to the rightmost position.
4. Press and hold the SET key for 1.5 seconds again.
Setting is complete when the display blinks.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500