• No : 21427
  • Release Date : 2018/08/22 16:27
  • Print

Indication of potentiometer on operation panel

When I raise the frequency using the potentiometer on the operation panel, indication stops at 61.12.
How can I raise it (up to around 90.00)?
Category : 

Answer

The potentiometer on the operation panel is initially calibrated so that the maximum indication is slightly over 60 Hz with the potentiometer turned to the maximum position.
You need to calibrate Pr.923 so that it indicates 90 Hz at the maximum position.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500