- No : 21435
- Release Date : 2018/08/22 16:27
-
Print
FR-A5CN
I want to install the heat sink outside the enclosure using the FR-A5CN, but the environment is bad and it is exposed to the spray of water there.
What should I do to provide a waterproof measure in this case?
- Category :
-
Answer
When the heat sink is outside, since the heat sink and fan are not waterproof, you need to enclose them so that they are not exposed to the spray of water.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- Option