• No : 21462
  • Release Date : 2018/08/22 16:27
  • Print

Connecting potentiometer

I have two FR-V220E-5.5K units and I want to use them with a single external potentiometer for variable speed control.
Do you have a connection example?
Category : 

Answer

Connect the external potentiometer to the terminals 10, 2, and 5 of the first inverter (be sure to connect the variable terminal to the terminal 2). Connect the terminals 2 and 5 of the first inverter to the terminals 2 and 5 of the second inverter using wires. Figure 1
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200