• No : 21506
  • Release Date : 2018/08/22 16:28
  • Print

UL standard certification number

What are the UL standard certification numbers of the FR-E500, FR-A500, and FR-A200?
Category : 

Answer

The UL standard certification numbers (UL Listing Card No.) of the FR-E500, FR-A500, and FR-A200 are as follows:

FR-A200 series??????E131592
FR-A500 series??????E131592
FR-E500 series??????E131592

The same number for all three series.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-A200, FR-A500