- No : 21521
- Release Date : 2018/08/22 16:28
-
Print
FR-E520 7.5 kW model
What are the outline dimensions of the above model? This model is not listed on your catalog.
Currently, I use the FR-A520 as the 7.5 kW inverter.
If the FR-E520 is smaller and less expensive, I want to adopt it.
- Category :
-
Answer
The outline dimensions of the FR-E520-7.5K are 180W×260H×170D.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500