- No : 21542
- Release Date : 2018/08/22 16:28
-
Print
Connecting operation panel to enclosure
Which cable should I use to connect the operation panel to the enclosure?
What is the maximum cable length in this case?
- Category :
-
Answer
To connect the operation panel to the enclosure, use the parameter unit connection cable FR-CB201, FR-CB203, or FR-CB205. The maximum cable length is 5 m.
Note that you need the control panel rear cover and adapter set to connect the operation panel to the enclosure.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500