• No : 21555
  • Release Date : 2018/08/22 16:28
  • Print

Control cable between high power factor converter and inverter

Are the high power factor converter and inverter directly connected with a control cable?
Or, is a relay required between them?
Category : 

Answer

Connect the high power factor converter and inverter directly with a control cable, without using a relay. Since a fast-response is required to shut off the inverter output by the RDY signal, and placing a relay delays the response. (Therefore, you can use the relay for the RSO signal.)
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option