• No : 21571
  • Release Date : 2018/08/22 16:28
  • Print

Size

How large is it?
Category : 

Answer

The high power factor converter itself is almost same size as general-purpose inverter with the same capacity (FREQROL-A200 series), however, an additional space to install accessories (outside box, reactor 1, and reactor 2) is required.

The ratio between the installation spaces for the converter and accessories is approximately 1:1.5.
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option