• No : 21591
  • Release Date : 2018/08/22 16:28
  • Print

What type of personal computer is required?

What type of personal computer is required?
Category : 

Answer

The PC platform can be PC98 or DOS/V as far as Windows 3.1 or Windows 95 runs smoothly, with free space of 1 MB or more on the hard disk, and memory (RAM) 1 MB or more.
To install the software, one or more 3.5-inch floppy disk drive are required.
A mouse and serial port are also required.
Product Name
Inverter, magnet motor drive
Product Category
Inverter communication software
Series
Engineering software