• No : 21612
  • Release Date : 2018/08/22 16:28
  • Print

Can a brake resistor or brake unit be connected?

Can a brake resistor or brake unit be connected?
Category : 

Answer

You can connect them to the FR-A024 inverter 0.4 to 3.7K. (You cannot connect them to 0.1K and 0.2K.)Available brake resistor options include the FR-ABR high-duty brake resistor, MRS, and MYS brake resistor.
The brake unit can be connected to all capacity types.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024