• No : 21632
  • Release Date : 2018/08/22 16:28
  • Print

Compatibility of plug-in option

Can I use the plug-in option used with the FR-A100 with the FR-A100EXCELLENT?
Category : 

Answer

Use the plug-in option dedicated for the FR-A100EXCELLENT.
To avoid an incorrect installation, the connector position for the plug-in option and the FR-A100EXCELLENT is different from the one for the FR-A100 plug-in option.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.

The functions of the FR-EPB to FR-EPE are the same as those of the conventional FR-APB to FR-APE options.
For the FR-A100EXCELLENT, the FR-EPG and FR-EPH options are added.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
FR-A100