• No : 21761
  • Release Date : 2018/08/22 16:29
  • Print

FR-PA07

I want to give the start command from an external switch and set the frequency using the setting dial on the optional enclosure surface operation panel FR-PA07 as using the potentiometer.
I want to operate the inverter at 80 Hz.
1. Which parameter setting is required for this purpose?
2. Can I display the rotations per minute instead of frequency?
Category : 

Answer

1. Press the PU/EXT key on the operation panel FR-PA07 to choose the PU operation mode.
Set Pr.161 (Frequency setting/key lock operation selection) to "1" and Pr.79 (Operation mode) to "3".
To limit the maximum frequency to 80 Hz, set Pr.1 (Maximum frequency) to "80 Hz".
2. Set Pr.37 (Speed display) to the rotations per minute at 60 Hz.
Note that you cannot stop operation and set the frequency using the operation panel of the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ