- No : 21774
 
      - Release Date : 2018/08/22 16:29
 
        - 
          
              Print
          
        
 
  
 
Display unit of operation panel
    
      I want to change the display unit of the operation panel from frequency to rotations per minute.  
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Set the rotations per minute that is obtained while operating at the frequency set with Pr.505 (Speed setting reference) to Pr.37 (Speed display).
For example, when Pr.505 = 50 Hz and Pr.37 = 1500 and the running frequency is 50 Hz, the running speed monitor shows "1500".
However, if Pr.144 (Speed setting switchover) = 0, the display value remains as frequency.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-F700PJ, FR-A700, FR-F700P