- No : 21924
- Release Date : 2018/08/22 16:30
- 
          
              Print
          
        
 
Device Net classes
    
      I do not understand the meanings of some terms used in the Instruction Manual of the Device Net.
1. Class
2. Instance
3. Attribute
I often see these three terms.
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Class, instance, and attribute represents different grouping of objects.
Comparing object grouping to a mailing address, they can be considered as follows:
State (= class), city (=instance), and town (= attribute)
For inverter control, available parameters and operation commands are grouped into classes.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Plug-in option
        - Series
- FR-F500, FR-A500