• No : 21966
  • Release Date : 2018/08/22 16:30
  • Print

Fault output terminal load pattern

Are the fault output terminals A and C, and B and C of the power regeneration converter FR-RC capable of a micro load of 5 VDC±5%, 10 mA?
Category : 

Answer

The fault output terminals A and C, and B and C of the power regeneration converter FR-RC are not capable of a micro load of 5 VDC±5%, 10 mA. The minimum load pattern is 5 VDC, 100 mA.
Product Name
Inverter, magnet motor drive
Product Category
Power regeneration converter
Series
Option