• No : 22017
  • Release Date : 2018/08/22 16:30
  • Print

Control wire of FR-HC RDY signal

Is the contact between the terminals RDY and SE a NO contact or NC contact?
Category : 

Answer

The contact between the terminals RDY and SE is open collector output.
Operation is:
Normal: Non-conductive
Fault: Conductive
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option