- No : 22036
- Release Date : 2018/08/22 16:30
-
Print
Position control
I am considering how to control positioning of equipment that moves horizontally.
What are the pros and cons of using vector inverter, servo motor, and stepping motor?
- Category :
-
Answer
The servo motor provides the highest precision and response.
With the vector inverter, position control using pulse train input ensures position control at precision of encoder resolution ±1 pulse.
However, since the motor inertia is large, the response is lower than the servo motor.
The stepping motor uses open-loop control and precision equivalent to the servo motor cannot be expected, and also loss in synchronism may occur.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200