• No : 22038
  • Release Date : 2018/08/22 16:30
  • Print

FR-CV

What is the proper use of the FR-CV and conventional FR-RC and FR-HC?
Category : 

Answer

Use the FR-HC to suppress harmonics. It also supports power supply regenerative driving.
The FR-CV and FR-RC are both power supply regeneration units.
The differences are:
The FR-CV allows for connecting multiple inverters. The FR-RC allows for connecting only one inverter.
The FR-CV can produce 100% regenerative torque with the same capacity as the inverter.
(The FR-RC can only produce 75% torque depending on the capacity.)
Product Name
Inverter, magnet motor drive
Product Category
Power regeneration converter
Series
Option