• No : 22050
  • Release Date : 2018/08/22 16:30
  • Print

CC-Link

While the FR-E520 has the CC-Link model, the FR-E540 does not have the CC-Link model according to the catalog.
When do you plan to have the 400 V class that supports CC-Link?
Category : 

Answer

Already released.
Unlike the E520, you need to purchase the optional card FR-E5NC.
Product Name
Inverter, magnet motor drive
Series
FR-E500