• No : 22058
  • Release Date : 2018/08/22 16:30
  • Print

Separation of operation panel

The operation panel of the E500 series can be removed and installed to another device with the back cover attached. Does S500 series also allow for separation of the operation panel?
Category : 

Answer

The operation panel of the FR-S500 is not detachable.
For the FR-S500-○○K-R (compatible with RS-485 communication), you can install the FR-PU04 on the enclosure surface by purchasing the FR-PU04 and PU cable.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-S500