- No : 22081
- Release Date : 2018/08/22 16:30
-
Print
Which motors can I use with the inverter?
Let me know which types of motors I can use with the inverter.
Which should I choose from various types of motors (for example, geared motors, induction motors)?
- Category :
-
Answer
You can use general-purpose three-phase induction motors.
You can also use geared motors if the motor itself is an induction motor.
Synchronous motors are not recommended due to possible synchronization loss.
Note that single-phase motors cannot be used.
- Product Name
- Inverter, magnet motor drive
- Series
- Others