- No : 22089
- Release Date : 2018/08/22 16:30
-
Print
Inverter stop-on-contact control
I want to implement stop-on-contact control with the inverter.
I also want to connect the inverter and programmable controller via CC-Link.
Can I realize both of them simultaneously?
- Category :
-
Answer
Use the FREQROL-A500 series inverter with the optional FR-A5NC.
Then, you can implement both of stop-on-contact control and CC-Link operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500