• No : 22492
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 10:01
  • Print

Setting the MELSEC iQ-R series inter-module synchronization function

How can I set the MELSEC iQ-R series inter-module synchronization function?
Category : 

Answer

Set modules in a module configuration diagram with GX Works3 and configure the inter-module synchronization setting.

[Navigation Window] -> [Parameter] -> [System Parameter] -> [Synchronization Setting within the Modules]
Set each item as follows.

Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series