• No : 22542
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 15:05
  • Print

Difference between C Controller module and programmable controller CPU module

What are the differences between C Controller module and programmable controller CPU module?
Category : 

Answer

- C Controller module:
  Programs are created using C and C++ languages.
  The programs run based on each task and parallel processing of multiple tasks based on priorities is possible.
  It is suitable if there are past C language program resources (such as programs created for using microcomputers
  and personal computers) or the programs handle relatively large data or process complicated arithmetic expressions.

- Programmable controller CPU module:
  Programs are created using ladder diagrams, lists, SFC, and Structured Text.
  The programs are controlled in the repetitive operation of stored program (sequence control).
Product Name
MELSEC-Q Series
Series
CPU