- No : 22573
- Release Date : 2018/09/03 17:29
-
Print
Auto refresh setting in GX Configurator -MB
What is auto refresh setting in GX Configurator -MB for MODBUS (R) interface module?
- Category :
-
Answer
Auto refresh setting is for storing the buffer memory data of a MODBUS (R) interface module to specified devices of a CPU module and for storing device data of the CPU module to the buffer memory automatically.
Auto refresh setting is required when the master function is used, but not required when only the slave function is used.
- Product Name
- MELSEC-Q Series
- Series
- MODBUS