When trying to start the simulation function, the following error appears. Are there any remedies?
Communication with PLC cannot be established. The possible causes are as follows. Refer to manuals or other related instructions.
- Faulty cable (faulty connection, break)
- The PLC power is OFF or in the reset state.
- Faulty hardware in the power module, CPU module, I/O modules, intelligent module, network module, base unit,
or extension cable in use
<ES: 01808201>