FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
>
Clock function accuracy
Back
No : 22651
Release Date : 2018/09/03 17:29
Update : 2018/09/26 16:53
Print
Clock function accuracy
What does the following information on the basic model QCPU's clock function denote?
- Accuracy: -2.57 to +5.27s(TYP.+2.22s)/d at 25 degrees Celsius.
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
Answer
It means that in an ambient temperature of 25 degrees Celsius, an error per day falls within the range of "delay of 2.57s" to "advance of 5.27s".
"TYP.+2.22s" denotes that the standard value is "advance of 5.27s".
Product Name
MELSEC-Q Series
Series
CPU