Products earlier than version 8.58L do not support a project in which the following parameters are set. All the parameters are set to their default values before the project is read.
- Remote I/O
Projects in which "PLC Operation Mode at H/W Error" is set to "Continue" in the "Intelligent Function Module Detailed Setting
" window for the I/O assignment setting
- Universal model QCPU modules (Q02U, Q03UD, Q04UDH, Q06UDH)
Projects in which local devices are set in the "File Usability Setting" window for the program setting