• No : 22706
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 14:33
  • Print

Replacing personal computers with C Controller modules

What are the merits in replacing a personal computer with a C Controller module?
Category : 

Answer

The merits are as follows.

(1) Downsized device
      The volume ratio is 1 to 10 in comparison with the VME card rack (6U) type.
(2) Long-term stable supply
      Anxiety about the supply and production discontinuation of the components, necessary for frequent specification changes
      and hardware changes of boards, is relieved.
(3) Improvement in environmental resistance
      Thermal and vibration durability is improved.
(4) The OS is replaced with a proven embedded OS and thus stable operation is performed.
(5) Users can free themselves from the task of selecting boards and software to keep up with updates on the version of the OS
      for personal computers (Windows).
(6) The hard diskless design reduces failures.
Product Name
MELSEC-Q Series
Series
CPU