• No : 22718
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/18 11:45
  • Print

Ethernet system configuration of a redundant system

What will the system configuration be when a host OPS is connected to a redundant system via Ethernet?
Category : 

Answer

The following figure shows the basic configuration.



When a control system Ethernet module is faulty or disconnected, the system is switched at a disconnection and the module is connected to a standby system.
In this configuration, when a LAN card of a personal computer, hub, or a LAN cable between them is disconnected, the communication between the computer and a programmable controller will be disabled.

To prevent this problem, insert two LAN cards into the personal computer and configure two Ethernet systems as shown in the figure below.

Product Name
MELSEC-Q Series
Series
CPU