- No : 22721
- Release Date : 2018/09/03 17:29
-
Print
Hardware setting for using Q series extension base units
Do I need to configure any hardware setting to use Q series extension base units?
- Category :
-
Answer
You need to set the number of extension base units with the connector for setting the number of extension base units.
For details, refer to the following.
SH-080473 QCPU User's Manual (Hardware Design, Maintenance and Inspection)
4.3 Connecting an Extension Base Unit
- Product Name
- MELSEC-Q Series
- Series
- CPU