- No : 22767
- Release Date : 2018/09/03 17:30
-
Print
PLC write not possible due to memory overload
When I tried to write a comment to the program memory in LCPU, it failed due to memory overload. What is the remedy?
- Category :
-
Answer
If comments cannot be stored in the program memory, write them in the standard ROM or a memory card.
Calculate the memory capacity in GX Works2 or GX Developer before performing PLC write to check whether it is possible to write all data to the program memory.
- Product Name
- MELSEC-L Series
- Series
- CPU