• No : 22786
  • Release Date : 2018/09/03 17:30
  • Print

SD1286 of LCPU with built-in Ethernet port

During socket communication of L series CPU with built-in Ethernet port, how does the special register SD1286 (Receive state signal) correspond to the connection number?
Category : 

Answer

The bits 0 to F of the special register SD1286 (Receive state signal) correspond to the connection numbers 1 to 16. When it receives data, the corresponding bit will turn ON.
Product Name
MELSEC-L Series
Series
L Series