- No : 22790
- Release Date : 2018/09/03 17:30
-
Print
Built-in positioning function of LCPU
What is the built-in positioning function of LCPU?
- Category :
-
Answer
The positioning operation starts just in 30 microseconds, with a maximum high speed output of 200k pulses per second. S-curve acceleration/deceleration is also supported for applications that require machine vibration reduction.
For more details, refer to "POSITIONING FUNCTION" of "MELSEC-L CPU Module User's Manual (Built-in I/O Function)".
- Product Name
- MELSEC-L Series
- Series
- CPU