- No : 23009
- Release Date : 2018/09/03 17:31
-
Print
Clearing data in the QJ71C24N's receiving area buffer memory
Is it necessary to perform a zero clear write operation to the QJ71C24N series buffer memory in order to receive data again after received data is stored in the buffer memory address 600H/A00H and the following addresses?
- Category :
-
Answer
Receiving data overwrites the buffer memory data. Writing 0 with a program can be performed but is unnecessary as the data is overwritten.
- Product Name
- Network Related Products
- Series
- Computer Link / Serial Communication