- No : 23063
- Release Date : 2018/09/03 17:31
-
Print
Limitation on the number of MELSOFT products that can be connected with the QJ71E71
What is the maximum number of the MELSOFT products I can connect with the QJ71E71 series?
- Category :
-
Answer
In the TCP/IP connection, you can connect up to 17 MELSOFT products at the same time using a dedicated connection for system and the connections for users 1 to 16. In the UDP/IP communication, you can connect multiple MELSOFT products and GOTs using a dedicated connection for system.
- Product Name
- Network Related Products
- Series
- Ethernet Interface Module