The SLMP communication frames supported by the FX5-CCLGN-MS are 3E and 4E frames.
When SLMP communication is performed from an SLMP-compatible device to the FX5-CCLGN-MS, communication can be performed by setting the destination port to the SLMP communication port number of the FX5-CCLGN-MS in the settings of the SLMP-compatible device.
(Transmission requests from FX5-CCLGN-MS to SLMP devices are not allowed.)
For the port number to be set, please refer to the following manual.
MELSEC iQ-F FX5 User's Manual (CC-Link IE TSN)