FX5-CCLGN-MS supports 1 Gbps communication speed with firmware version: 1.010, and 1 Gbps and 100 Mbps communication speed for version 1.010.
If the communication speed of FX5-CCLGN-MS is set to 1 Gbps, communication will not be established if an inverter with a communication speed of 100 Mbps is directly connected. Use a CC-Link IE TSN Class A-compatible switching HUB to convert the communication speed.
*Check the CC-Link Association website for recommended switching HUBs.