• No : 39284
  • Release Date : 2023/01/12 16:50
  • Print

Regarding the switching Hubs that can be used for CC-Link IE TSN

Which switching HUBs can be used with CC-Link IE TSN?
Category : 

Answer

The CC-Link IE TSN has a CC-Link IE TSN Class B/A, and the available switching HUBs are also specified by supported standards, synchronization accuracy, etc.
Check the CC-Link Association website for the model name and usage of the corresponding switching HUB.
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series