PLC :it is written to the CPU module and consumes the number of steps.
・Without character - 3 steps
・With character : 4 + (Number of characters + 2 + 14) / 15 + Number of characters (steps)
Peripheral : Not written in the CPU module and is saved as additional program information.
・One line consumes one step.
・An asterisk (*) is automatically placed in front of the entered text.