It is possible to connect to the cloud: MQTT broker (server) using the MQTT communication function of FX5-ENET.
The MQTT communication function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later